Vous pouvez aussi nous contacter en nous appelant au:
En ligne : 24 Jan 2006
Lambda has added a new 3.3kW version of its successful Genesys™ range of rack-mountable, programmable power supplies. Offering one of the highest power densities available in a compact 2U unit and complementing the already highly successful 1U 1500W and 750W versions, Genesys™ continues to set the standard for flexible, reliable, AC/DC power systems for OEM, industrial, ATE, test and laboratory applications. RoHS compliance is standard allowing both exempt and non-exempt applications to be addressed.
The first group of 3.3kW models released include output voltage ranges of 0-8, 0-60, 0-150 and 0-600V. Maximum output current for the lowest voltage range is 400A. Further models will be released during the first half of 2006 to complete the full line up of 12 versions. Each model can be ordered with single phase 230VAC input or three phase (either 208V or 400V) and all units have active power factor correction.
The Genesys™ 3.3kW offers high reliability through its reduced part count, proven topologies screened components and Lambda de-rating guidelines. Common to the whole Genesys™ family is the RS232/485 interface which is built in as standard along with comprehensive analogue control and monitor interface. Options available include a new multi-drop version of the IEEE 488.2 interface card which requires only one IEEE address and only one option card to be fitted in the master unit to control up to 31 slave units via the RS485 link. This can be particularly beneficial for making test systems more noise immune. Systems designers will also benefit from the new global commands that will simplify programming and provide faster test sequence execution with multiple unit configurations. Isolated analogue interface option cards are also available.
Paralleling units for higher power is now simplified with the master unit able to report total system output current and rack space is minimised because all Genesys™ units are true “zero stack” with no space required between units.
CE marked in accordance with the Low Voltage Directive, Genesys™ conducted and radiated EMI conforms to EN55022-A, FCC-A . Safety approvals include UL60950 and EN60950.