In alternativa, puoi contattarci così:

TDK-Lambda News

Using constant current control for metal purification

Postato : 23 May 2013

TDK-Lambda's Z + and Genesys™ Programmable Power Supplies

TDK-Lambda's Z + and Genesys™ Programmable Power Supplies

In the vast world of power supply applications, we can identify two main categories for regulating the power applied to the load. The first being ‘constant voltage’, where the control loop maintains a constant voltage to varying load current demands and the second, ‘constant current’ where the current is maintained constant to vary the voltage applied to the load.

Since current flow is closely related to the flow of charge over time, having constant current control allows the user to control the speed of some chemical processes and in certain circumstances reverse it.

In industrial applications, the currents involved are often very high and generally require the current to be precisely regulated and accurately varied or controlled.

An industrial process widely used for the purification of metals (especially aluminium and copper) is electrolysis. The material to be purified is immersed in a ‘tub of electrolyte’, then a potential difference is applied between the sample to be purified. In figure 1, copper acts as the anode and the cathode is where the pure material is collected.

In this process, the amount of copper deposited or 'purified' is directly related to the applied current. The use of a constant current power supply allows the perfect control of the process.

These processes typically use currents in the order of thousands of Amps, low <5Vdc, operating voltages, and very high power. For example, 15MWh of electricity is needed to produce 1 ton of aluminium. The use of high-efficiency power supplies clearly creates significant savings in terms of energy bills and operating costs.

TDK-Lambda Solutions
TDK-Lambda is a world leader in technological research in the field of power supplies and has developed several ‘Constant Current’ power supply solutions.

The ZUP, Z + and Genesys™ allow full control of the current and the output voltage, as well as feedback on the same parameters. In addition, the availability of isolated interfaces, analogue, digital RS232/485, IEEE488 and LAN allows a high flexibility of integration and system control. The power ratings range from 200W to 15kW with the possibility of placing up to 4 units in parallel, to increase the power up to 60kW and output currents up to 4000A.

PAGE TOP

PAGE TOP