In alternativa, puoi contattarci così:
Questo pratico glossario viene periodicamente aggiornato e contiene la terminologia e le abbreviazioni relative ai prodotti per l’alimentazione elettrica. Seleziona una lettera per iniziare.
A B C D E F G H I J K L M N O P Q R S T U V W X-Z #Related to direct-current electricity or dc.
Separation of the signal/power source (or sink) in such a way that dc current cannot bridge the connection. There are two generally accepted methods for galvanic isolation: use of transformers or use of optical isolators. Both allow the ac component of a signal to pass, but not the dc component.
A parallel communications bus. Used to connect electronic test and measurement devices to control equipment (such as a computer). Also known as IEEE488. See Communications Port.
SI prefix multiplier. Multiplies by 109. So 100 GHz = 100 x 109 Hz. Written as 'giga'. Abbreviated to 'G'.
An unwanted transient voltage spike occurring on a signal.
Abbreviation of General Purpose Interface Bus.
A conducting connection, whether intentional or accidental, by which an electric circuit or equipment is connected to earth, or to some conducting body that serves in place of earth.
Schematic Symbol for Ground (or Earth)
A bus, grounded in at least one place, to which individual grounds in a system are attached.
Interconnected bare conductor arranged in a pattern over a specified area, laid out on or below the earth’s surface.
A condition that occurs when there is more than one ground connection path between two pieces of equipment or circuits. These multiple paths produce a similar effect to a loop antenna which will pick up and radiate interference.
1) A layer of copper on a PCB providing a low impedance ground return to all circuit elements needing it. Also for shielding.
2) A conductive surface serving as the circuit reference ground or as a near-field reflection point for an antenna.
A metal rod, usually copper clad, driven into the earth to serve as a ground terminal.
Connected to a common reference point (usually earth).