In alternativa, puoi contattarci così:
Questo pratico glossario viene periodicamente aggiornato e contiene la terminologia e le abbreviazioni relative ai prodotti per l’alimentazione elettrica. Seleziona una lettera per iniziare.
A B C D E F G H I J K L M N O P Q R S T U V W X-Z #Symbol for Impedance.
A diode that permits current to flow both in the forward direction (like a conventional diode) and in reverse direction. When current flows in the reverse direction, Zener diodes are designed to drop a specified amount of voltage (the Zener Voltage). They are used primarily to regulate the output voltage of low power regulators.
Schematic Symbol for a Zener Diode
The reverse voltage at which breakdown occurs in a Zener Diode.
SI prefix multiplier. Multiplies by 10-21. So 100 zF = 100 x 10-21 F. Written as 'zepto'. Abbreviated to 'z'.
SI prefix multiplier. Multiplies by 1021. So 100 ZF = 100 x 1021 F. Written as 'zetta'. Abbreviated to 'Z'.