2017
2017
SPS NUREMBERG - A STEP AHEAD FOR OUR MARKET RECOGNITION!
December 4th, 2017
We have successfully concluded our first presence in SPS (Nuremberg, Germany) - the most prestigious automation fair in Europe.
Our booth was visited by > 500 visitors. New business partnerships and opportunities were prospected.
There was high interest expressed for our innovative solutions integrated in the new products as:
- NDW240 - the first programmable 240W DC/DC converter that can convert any voltage 10…55Vdc in any voltage 5…56V, replacing several conventional models
- DCW20 - a digital DC-UPS that can be operated also as 960W DC/DC converter with multiple features
- NISO-20 - first DC/DC isolation module for DIN rail, rated 10…55V/800W
- NEF210 - an advanced 2 channels digitally controlled overcurrent protector, featuring outstanding management by ANDROID and Windows OS
- NPSM121IP / NPSM241IP - a compact solution for IP65 power supplies
- 36V models - for the NPSM241/481 families
- ”H” versions - increased surge protection (> 6kV) for NPSM121/241/481 and NPSW480 families
Our position as one of the most complete solution providers in the DIN rail power solutions was confirmed by many of our visitors.
Our innovative implementations were acknowledged as differentiating us in solving many applications in an efficient and original manner.
We thank all our visitors for the time they have spent in our booth and the opportunity to develop our collaboration!
October 12th, 2017
In the last few years NEXTYS has extended its presence on the international market by appointing new partners.
Through our local partner EVENT AUTOMATION DESIGN (www.event-automation.com) we have introduced our latest products to the important TIIE exhibition (17th Tehran International Industry Exhibition).
Located in a fast growing and promising market this fair represented an opportunity of presenting our innovative approach in the DIN rail power solutions.
There was an important number of visitors that showed interest in our products and launched queries about possible application in their systems.
This fair confirmed the good reception our solutions have in emerging and fast growing markets, based on the combination of innovation - performance - affordable cost.
We thank to all visitors and to our partner for the success of this introductory event.
January 19th, 2017
Most of the industrial solutions for DC/DC converters are based on an input voltage range and a fixed (or relatively limited) output voltage (e.g. 12, 24, 48Vdc, etc.). This approach generates many models, with all related consequences in terms of inventory, operational limits and cost.
NDW240 introduces a breakthrough concept for the DC/DC converters, following the “all-in-one” strategy that is broadly applied in our products.
NDW240 is a 240W, 3 kV isolated DC/DC converter that can convert any DC voltage 11 to 55V to any DC voltage 5 to 55V, with 10mV resolution, with a load rating of 240W/ max.10A.
The output voltage set-up can be done through the front panel or through a USB interface, operable by Windows or Android systems through our well-known application POWERMASTER.
NDW240 includes an ORing circuitry and various protections. It can be paralleled for power or redundancy.
NDW240 is aimed to replace the NDDxx family of traditional DC/DC converters, offering excellent price / performance ratio and improved features.
January 16th, 2017

In the last years NEXTYS has extended the digital solutions for the management of the power products.
We have introduced the control and regulation of several platforms by proprietary algorithms and achieved outstanding performance at reasonable cost.
We have added extensive communication features, either by USB or MODBUS, enhancing the integration capabilities of our products in intelligent systems.
The software suite POWERMASTER, aimed to remote monitoring and setup of the devices, was applauded by the market, especially after including the possibility of operation on Android systems.
The users will have the possibility to distinguish those products with digital implementation as bearing the logos POWERMASTER and DIGITAL POWER, as expressed in their data sheets.